Channel Setup

cdma2000 Configuration Summary Table

This section defines the Settings Current and Apply Needed buttons. Only one button is available at any time. These buttons are available in all of the cdma2000's tree nodes.

This button sets all channels to equal power, and the total power to 0 dB.

This button scales all of the current channel powers so that the total power equals 0 dB, keeping the previous power ratios between the individual channels.

[:SOURce]:RADio:CDMA2000[:BBG]:REVerse:PADJust EQUal|SCALe

Clicking on the Operating Mode tab in the main window allows you to access and configure the radio configurations listed below.

RadioConfig 1/2 Traffic

RadioConfig 1/2 Access

RadioConfig 3/4 Traffic

RadioConfig 3/4 Enhanced Access

RadioConfig 3/4 Common Control